Date Updated:Apr. 01. 2026
Moving the control panel of a machine tool horizontally【Workability & Maintenance】
There are units available that rotate the control panel horizontally.
By adjusting the control panel to an easy-to-see angle, work efficiency can be improved.▶You can pass the control panel wiring through the central hole of the swivel unit.


▶ A stand pipe for adjusting the height of control panels is also standardized for use in combination with the swivel mounts
“DKSF” and “DKSW”.

Recommended Products
Issue/case studies
Installation Method/Maintenance
Solution samples
Machine Elements