Nov. 08. 2023
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
Jan. 09. 2025
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
Apr. 08. 2024
What is a Swivel Mount?This is an introduction page for the swivel unit. We provide an easy-to-understand overview of what a swivel unit is, along with its types and features.Aug. 25. 2026 time >
This is an introduction page for the swivel unit. We provide an easy-to-understand overview of what a swivel unit is, along with its types and features.
Aug. 25. 2026 time >
Select the best screws for your needsThis page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etcJul. 06. 2026 time >
This page helps to select a Product based on application needs. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc. Vacuum, Low Outgas, Clean, Chemical Resistance, High Strength, Heat Resistance, etc
Jul. 06. 2026 time >
No. 2: Vacuum environmentsVacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments! Jul. 06. 2026 time >
Vacuum technology is often used in semiconductor manufacturing equipment. A vacuum is not required for all equipment. A vacuum would mainly be required for equipment that uses plasma or an electron beam. In Part 2, we introduce some NBK products that are ideal for use in these vacuum environments!
What are Socket Head Cap Screws (Bolts) ? Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc. Jul. 06. 2026 time >
Hex Socket Head Cap Screws (cap bolts) are bolts (screws) with hexagon-shaped holes in their heads. It lists product descriptions for hex socket head cap screws, recommended products, etc.
Miniature Screws/Precision Screws Lineup ListThis is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.Jul. 06. 2026 time >
This is the lineup list of miniature screws and precision screws. Select the product required from the lineup list.
Micro Screws: M0.6 (S0.6) to M2.6 LineupNBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space. Jul. 06. 2026 time >
NBK offers a wide-ranging lineup of small-diameter screws in various shapes and materials. Various head diameters and heights are available for the same screw diameters, contributing to saving space.
Washers: Essential Components for Secure Connections This page introduces washers. As well as a description of washers, the washer products handled by NBK are introduced. May. 26. 2026 time >
This page introduces washers. As well as a description of washers, the washer products handled by NBK are introduced.
May. 26. 2026 time >
No. 6: Thermal CyclingHere we discuss thermal cycling, which is often an issue in semiconductor manufacturing equipment. May. 26. 2026 time >
Here we discuss thermal cycling, which is often an issue in semiconductor manufacturing equipment.
Washer fall-out prevention is required 【Workability/Maintenance】Introducing integrated washer type screws.May. 26. 2026 time >
Introducing integrated washer type screws.
Hexalobular Internal Driving Feature for Bolts and ScrewsThis page describes JIS B 1015 "Hexalobular internal driving feature for bolts and screws".May. 14. 2026 time >
This page describes JIS B 1015 "Hexalobular internal driving feature for bolts and screws".
May. 14. 2026 time >
Monitors need to be movable with one touch in accordance with the worker's height or the nature of the work【Improved productivity/workability】Introducing parts enabling free adjustment of the monitor position.May. 01. 2026 time >
Introducing parts enabling free adjustment of the monitor position.
May. 01. 2026 time >
Simple positioning with vertical axes is needed 【Workability / maintenance】Introducing brackets that fix with button operation alone.May. 01. 2026 time >
Introducing brackets that fix with button operation alone.
Unified Coarse Screw Threads/Unified Fine Screw ThreadsThis page describes JIS B 0206 / JIS B 0208 "Unified Coarse Screw Threads/Unified Fine Screw Threads".Apr. 27. 2026 time >
This page describes JIS B 0206 / JIS B 0208 "Unified Coarse Screw Threads/Unified Fine Screw Threads".
Apr. 27. 2026 time >
Vol. 12 Back to Basics Series! Screw Reference DimensionsThe absolute ABCs, screw reference dimensions that are important when designing. A lot of problems can occur if you use the wrong dimensions when designing or placing an order. Nedzigon will explain screw terminology and use pictures to introduce the various thread types. Apr. 23. 2026 time >
The absolute ABCs, screw reference dimensions that are important when designing. A lot of problems can occur if you use the wrong dimensions when designing or placing an order.
Nedzigon will explain screw terminology and use pictures to introduce the various thread types.
Apr. 23. 2026 time >
No. 8: Preventing Part Fall-outAre you struggling with screw or washer fall-out during equipment assembly or maintenance? Here we introduce products that can be used to prevent part fall-out. Apr. 01. 2026 time >
Are you struggling with screw or washer fall-out during equipment assembly or maintenance? Here we introduce products that can be used to prevent part fall-out.
Apr. 01. 2026 time >
What are Captive Bolts (Screws)? Introduction of the NBK Captive SeriesNBK has standardized products for fall prevention of parts in the knob, pull and e-nedzi.com (special screw) categories. Use NBK's Captive Series for food machinery, packaging machinery and chemical manufacturing equipment that require CE Marking Compliance and Contamination Control. Apr. 01. 2026 time >
NBK has standardized products for fall prevention of parts in the knob, pull and e-nedzi.com (special screw) categories. Use NBK's Captive Series for food machinery, packaging machinery and chemical manufacturing equipment that require CE Marking Compliance and Contamination Control.
NEW SAVE