Mounting and MaintenanceThis page explains the mounting methods and maintenance for compact powerful magnets for FA. Details of the effects of air gap, surface roughness, and material are provided.Mar. 16. 2021 time >
This page explains the mounting methods and maintenance for compact powerful magnets for FA. Details of the effects of air gap, surface roughness, and material are provided.
Mar. 16. 2021 time >
Compact Powerful Magnet for FA - Terminology DescriptionThis page explains the terminology for compact powerful magnets for FA. Details regarding terminology for compact powerful magnets for FA such as adsorption and sliding load are provided.Mar. 16. 2021 time >
This page explains the terminology for compact powerful magnets for FA. Details regarding terminology for compact powerful magnets for FA such as adsorption and sliding load are provided.
Needs to reduce the time for setup jobs on the line【Automation / robots / motorization】Introducing case studies where instead of using operating handles, automatic positioning is used to reduce the working time.Aug. 25. 2020 time >
Introducing case studies where instead of using operating handles, automatic positioning is used to reduce the working time.
Aug. 25. 2020 time >
Only takes two minutes to understand!Wireless Positioning Units Installation/Connection MethodThe Wireless Positioning Unit can easily replace handles.The mounting and connection methods are introduced in videos.Aug. 25. 2020 time >
The Wireless Positioning Unit can easily replace handles.The mounting and connection methods are introduced in videos.
FlexusAug. 03. 2020 time >
Aug. 03. 2020 time >
Advancements in Servomotor Coupling TechnologyAug. 03. 2020 time >
Machining marks must be prevented 【Energy-saving / reduced work-hours】Introducing case studies using couplings that reduce vibrations to prevent machining marks and reduce work hours.May. 14. 2020 time >
Introducing case studies using couplings that reduce vibrations to prevent machining marks and reduce work hours.
May. 14. 2020 time >
Servomotor hunting must be suppressed 【Productivity increase】Introducing case studies using couplings with excellent damping performance to improve productivity.May. 14. 2020 time >
Introducing case studies using couplings with excellent damping performance to improve productivity.
Rotation shaft vibration must be suppressed 【Productivity increase】Introducing case studies using couplings that control vibrations to improve productivity.May. 14. 2020 time >
Introducing case studies using couplings that control vibrations to improve productivity.
Shaft radial load must be suppressed 【Automation / robots / motorization】Introducing case studies using couplings with excellent constant velocity and eccentric reaction force to suppress radial load on the shaft.May. 14. 2020 time >
Introducing case studies using couplings with excellent constant velocity and eccentric reaction force to suppress radial load on the shaft.
Small screws are required 【Compact / lightweight】Introducing a rich lineup of miniature screws and precision screws.May. 14. 2020 time >
Introducing a rich lineup of miniature screws and precision screws.
Screws with high strength are required even in environments where steel cannot be used 【Compact / lightweight】Introducing screws using stainless steel/titanium screws with strength equivalent to steel for space and weight saving.May. 14. 2020 time >
Introducing screws using stainless steel/titanium screws with strength equivalent to steel for space and weight saving.
Vibration of the machine must be prevented to maintain workpiece machining accuracy 【Productivity increase】Introducing case studies using couplings with high torsional stiffness and vibration absorption functions to improve productivity.May. 10. 2020 time >
Introducing case studies using couplings with high torsional stiffness and vibration absorption functions to improve productivity.
May. 10. 2020 time >
Disturbances / vibrations must be suppressed 【Safety / precautionary measures】Introducing case studies using couplings that suppress vibrations to prevent disturbances/vibrations.May. 10. 2020 time >
Introducing case studies using couplings that suppress vibrations to prevent disturbances/vibrations.
Couplings that support minimal outgassing and large eccentricity are required 【High sanitation / corrosion-resistant / clean】Introducing Oldham couplings using PEEK spacers to support clean/vacuum environments with heat resistance.May. 10. 2020 time >
Introducing Oldham couplings using PEEK spacers to support clean/vacuum environments with heat resistance.
Stable speed control of the raising / lowering shaft is required 【High rigidity / high accuracy】Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.May. 10. 2020 time >
Introducing case studies using couplings with high rigidity to stabilize speed control of the raising/lowering shaft.
NEW SAVE