Nov. 08. 2023
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
Jan. 09. 2025
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
Apr. 08. 2024
No. 8: Preventing Part Fall-outAre you struggling with screw or washer fall-out during equipment assembly or maintenance? Here we introduce products that can be used to prevent part fall-out. Apr. 01. 2026 time >
Are you struggling with screw or washer fall-out during equipment assembly or maintenance? Here we introduce products that can be used to prevent part fall-out.
Apr. 01. 2026 time >
What are Captive Bolts (Screws)? Introduction of the NBK Captive SeriesNBK has standardized products for fall prevention of parts in the knob, pull and e-nedzi.com (special screw) categories. Use NBK's Captive Series for food machinery, packaging machinery and chemical manufacturing equipment that require CE Marking Compliance and Contamination Control. Apr. 01. 2026 time >
NBK has standardized products for fall prevention of parts in the knob, pull and e-nedzi.com (special screw) categories. Use NBK's Captive Series for food machinery, packaging machinery and chemical manufacturing equipment that require CE Marking Compliance and Contamination Control.
Moving the control panel of a machine tool horizontally【Workability & Maintenance】Introducing a unit that rotates the control panel horizontally.Apr. 01. 2026 time >
Introducing a unit that rotates the control panel horizontally.
Explanation of TerminologyCoupling, Explanation of Terminology Feb. 25. 2026 time >
Coupling, Explanation of Terminology
Feb. 25. 2026 time >
Description of Tamper Resistant Screws & Security Screws (Bolts) for the EngineersThis is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.Jan. 27. 2026 time >
This is the page on tamper-resistant screws in "Description of Special Screws for Designers." We introduce here what tamper-resistant screws are, the advantages of their use, various usage examples, and their types and characteristics.
Jan. 27. 2026 time >
How to Install Couplings:Alignment and Shaft Insertion LengthHow to Install Couplings:Alignment and Shaft Insertion LengthDec. 22. 2025 time >
How to Install Couplings:Alignment and Shaft Insertion Length
Dec. 22. 2025 time >
Slip Torque of Coupling – Set Screw TypeThis page explains the slip torque for set screw type couplings.Nov. 26. 2025 time >
This page explains the slip torque for set screw type couplings.
Nov. 26. 2025 time >
Galling and SeizingThis is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.Nov. 25. 2025 time >
This is a phenomenon that occurs while tightening, where the surface of the screw thread melts or welds due to frictional heat and the screw stops moving. To resolve galling, NBK's special surface treatment screws, such as those with fluorine coating, are recommended.
Nov. 25. 2025 time >
Special Surface Hardened ScrewsSpecial Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.Nov. 25. 2025 time >
Special Surface Hardened Screws, Seizing Prevention and Axial Force Stabilization., No Lubricant.
Increased degree of vacuum in equipment is required 【Productivity increase】Introducing screws which support use with vacuum equipment.Nov. 25. 2025 time >
Introducing screws which support use with vacuum equipment.
No. 1: The Semiconductor Industry and NBKAlong with the dramatic worldwide growth of semiconductors, similar development has taken place for semiconductor manufacturing equipment. For many years, NBK has developed and sold products for semiconductor manufacturing equipment.In Part 1, we introduce trends in the semiconductor industry, and describe some interesting efforts by NBK! Nov. 25. 2025 time >
Along with the dramatic worldwide growth of semiconductors, similar development has taken place for semiconductor manufacturing equipment. For many years, NBK has developed and sold products for semiconductor manufacturing equipment.In Part 1, we introduce trends in the semiconductor industry, and describe some interesting efforts by NBK!
What are Couplings? Explanation of Coupling Types and CharacteristicsA coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.Nov. 12. 2025 time >
A coupling is a mechanical component designed to transmit torque by connecting a drive shaft to a driven shaft.
Nov. 12. 2025 time >
Select Based on ApplicationSelect Coupling based on application Nov. 10. 2025 time >
Select Coupling based on application
Nov. 10. 2025 time >
Points to Consider When Mounting DisplaysWe describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.Oct. 29. 2025 time >
We describe the Mounting Systems for Display, which allow mounting of tablet PCs and displays in various locations on devices and equipment. This discussion will make clear to you the need for "solidity" and "flexibility" in mounting.
Oct. 29. 2025 time >
RoHS compatible all-stainless steel couplings are required 【High sanitation / corrosion-resistant / clean】Our abundant lineup allows us to ship highly reliable products with short lead times.Oct. 29. 2025 time >
Our abundant lineup allows us to ship highly reliable products with short lead times.
Screws in places unreachable by hand need to be tightened 【Workability / maintenance】Introducing a product for holding screws with excellent workability.Oct. 29. 2025 time >
Introducing a product for holding screws with excellent workability.
NEW SAVE